3/18/2017 8:35 PM | |
Posts: 16 Rating: (0) |
Dear sir how I can shutdown siemens 840d win win95 thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/20/2017 3:42:32 PMNew subject after splitting |
|
3/22/2017 3:43 AM | |
Joined: 10/17/2007 Last visit: 10/17/2024 Posts: 4047 Rating: (355) |
My answer is just shut off m/c power.. as I know you are talking about shut off MMC102 or MMC103. at beginning version of MMC102/MMC103, Siemens did not add soft key "Exit"--you only can shut of power--that will cause Win 95 or Win 98 not safe shut off, next time power up MMC will show blue screen and system scan HDD, I think Siemens add "Exit" to let user safety shut down Windows before power off the whole m/c.That may be starting from MMC103 Ver 4.4. you can try like this--in "StartUP" area , make sure you input password SUNRISE, then use extension key ">" to see if there is "Exit"--if yes, you are lucky, press it --then wait until screen showing not you can safety shout off windows
|
If you like my comments please |
|
Follow us on