4/20/2017 4:00 PM | |
Joined: 3/28/2017 Last visit: 7/8/2024 Posts: 79 Rating: (0) |
Hi, Where in the application can I check how many users can use webnav at once ? Thanks. |
4/20/2017 4:26 PM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating: (191)
|
WebNavigator client No license is required for the PC on which the WebNavigator client is running, as server licenses are available on the WebNavigator server. WebNavigator server As a prerequisite for the WinCC basic system, the WinCC RT basic license is required. No WinCC server license is required if no local WinCC clients are to be operated. Even when operating a WinCC client as a dedicated web server, you do not require a WinCC server license for the WinCC client. Licenses are available for 1 / 3 / 10 / 30 / 100 clients. If you have upgraded a WebNavigator version prior to V7.4, there may also be licenses for 5 / 25 / 50 / 150 clients. The packages are version-independent and can be combined. Up to 150 clients can access the WebNavigator server simultaneously. A message will appear if the number of licensed clients is exceeded during a login attempt by a WebNavigator client. No further logins will be possible. Source: |
Last edited by: Thunderstorm at: 4/20/2017 4:28:32 PMLast edited by: Thunderstorm at: 4/20/2017 4:33:20 PMSIMATIC PCS 7 - Overview |
|
Follow us on