5/5/2017 4:14 PM | |
Joined: 8/26/2016 Last visit: 4/4/2024 Posts: 31 Rating: (1) |
I'm agree, i try to fix the StartOpenness project syntax error. I succes, but even with a working code must be run as administrator and it seem it can reconize the my user as a member of the "Siemens TIA Openness" When is not the code is the integration of the SP1. I try to fix the "TiaPortalOpennessDemo_V14" but a lot of type who was virtual is now define ( the easy to fix) and some of the type completly disapear, so i need more information about how to use the new Openness. At least give a working demo so i can compare... P.J.:Here my working project StartOpenness tell me if you can start it. thx AttachmentStartOpenness.zip (443 Downloads) |
Follow us on