5/29/2017 8:06 AM | |
Posts: 41 Rating: (0) |
Hi all. I need help to try to auto tune my Y axis motor. with a 840D control sw v4.4 and I have never done this kind before with a Siemens control. I can see there is many ways to auto tune but I am confused to what I have to input on the of values. my Y axis motor data looks as follows 1FT6064-xAH7x-xxx 1303 4500 rpm 9,5 Nm 9,1 A I have attached pictures of my M/C screen where the tuning sektion is. I have tried to search for how to tune a motor but the controls that mention this is way newer that mine. please see attached pictures. best regards Flemming Attachmenttuning screen shots.zip (114 Downloads) |
6/2/2017 11:34 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Are you commissioning new machine or you want to tune motor which is replacement motor? From the alarm description in the attached snaps, it looks like you are trying to tune linear motor where as in MD it has been configured as rotary motor. So please check relevant axis data. Please refer the attached sheets, (extracts from Siemens manual) HTH. Attachment840D Drive tunning.pdf (270 Downloads) |
Follow us on