5/4/2017 6:31 PM | |
Joined: 2/2/2017 Last visit: 4/27/2024 Posts: 36 Rating: (4) |
I need to create shared libraries, but it seems that Eclipse manages only executable projects for IOT2000. How to create a shared library? Regardss ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/5/2017 2:02:14 PMNew subject after splitting |
|
5/11/2017 7:49 PM | |
Joined: 2/2/2017 Last visit: 4/27/2024 Posts: 36 Rating: (4) |
Hi, no one can help me? |
5/12/2017 8:19 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, with our Eclipse PlugIn it is only possible to create C/C++ projects. You can use the "normal" way in Eclipse to create a shared library (http://linuxtortures.blogspot.de/2012/02/shared-libraries-with-eclipse.html) and add our linkers and compilers. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
7/27/2017 3:47 PM | |
Posts: 5 Rating: (0) |
HI, Bergmanu, If I got a shared lib from others, like "libxxx,so", could I just copy it to my SDK location.../usr/lib,and use it? It seems to be some linking problems here, I 'm stuck in it for days. Because the arguments setting of IOT compiler and Linker is a little different from cross gcc linker. https://support.industry.siemens.com/tf/ww/en/posts/snap7-iot-for-quark-iot2000-platform/158392/?page=1&pageSize=10#post693778 |
Follow us on