9/9/2017 6:12 AM | |
Posts: 6 Rating: (0) |
hai everyone, I have s7 300 plc CPU314c 2 PN/DP, and also have s7 300 MPI adapter. when i connect adapter with PC it shows USB not recognised error (PFA). I open simatic manager as administrator, and create new project (didnt select any CPU model) and try to get programs from PLC to PC. When i click upload symbol it shows a pop up window asking rack and slot number(both are showing default value as 0). MPI address column is empty. i try to view configuration by clicking VIEW button in same window, i got ONLINE: Sin_Serve not started. also i couldnt locate such file in my drive. Kindly suggest me how to resolve the issue. My OS - Windows 64bit Vista Simatic manager - V5.5 + SP4 ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/11/2017 1:14:34 PMNew subject after splitting |
|
Follow us on