11/5/2017 5:46 AM | |
Posts: 16 Rating: (1) |
Dear experts I want to replace channel drives in a higher version software with another type of channel driver, I want to know if there is a way instead of deleting older one and placing new one. A way that can replace blocks automatically. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/6/2017 8:11:48 AMNew subject after splitting |
|
11/6/2017 12:24 PM | |
Joined: 10/26/2011 Last visit: 11/11/2024 Posts: 762 Rating: (192)
|
Hello, in PCS 7 the channel blocks are updating via updating the PCS 7 library or PCS 7 version. Updating only the channel blocks is Or do you mean updating of add-on libraries or additional channel blocks, like SIWAREX? |
SIMATIC PCS 7 - Overview |
|
Follow us on