7/27/2017 11:23 AM | |
Posts: 1 Rating:
|
Running PCS 7 V8.0 sp2, with WinCC V7.2. OS Servers, clients and redundancy working fine, we leave the runtime graphic view open on the servers. The servers are configured with WinCC OPC as OPC Server to which two different3rdparty OPC Client applicationsconnect. Yesterday the external OPC Clients applications experienced some lag in speed, and I suggested they restart OS 1 Server application which is selected as the Master OPC Server via the 3rdparty OPC Client applications. As soon as runtime was started it displayed the message ‘Start Screen not found’. You cannot select any picture from the selection box, although all the pictures are displayed within the browser none ‘can be found’ via the runtime selection window /box. Graphics can be found in WinCC Explorer and can be opened in Graphics viewer. Start picture has been defined in runtime properties within the project settings. OS Server 2 is still working fine, I am currently running OS Server 1 with ‘No Graphics runtime’ and although it seems to work fine- I am a bit anxious switching WinCC Clients over to OS Server 1- thus redundancy is currently highly debateable. |
This contribution was helpful to
1 thankful Users |
11/29/2017 11:22 PM | |
Posts: 1 Rating:
|
Hi, CS00. I have the same software version and system configuration. And the same problem. How did you solve it? |
Follow us on