5/19/2018 8:49 AM | |
Joined: 9/9/2015 Last visit: 10/8/2024 Posts: 727 Rating: (278) |
Hi trixon21, There are few possibilities. 1st, you could study the block in your simulation environment, trigger all the bit and see whether the valve positions of V0 - V1 change or not. 2nd way is , you could go to the block icon, swapped the V90 and V180 by yourself (my preferred way), name it a new block icon, number "5" , and assign it in you 2WayVlv Block . (the problem is in the faceplate, you could change it too if all the valve in your project behave the same, if not, you might need to have other solutions.) Last time when i deal with 2 ways valves, the valve actuator is using normal open/close/stop actuator. When the actuator at the field, opened, it goes to 1st direction, and closed, to the 2nd direction. Since it has only opened and closed signals, my takes last time was design a block icon but using back the block VlvPosL for 2 ways valves. For the faceplate, i remain the same. Hope it helps. Attached with a screenshot for you to have a better understanding. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on