7/9/2018 8:59 AM | |
Posts: 2 Rating: (0) |
Hi I'm Ajeng. I'm currently working on SINUMERIK 828D and I want to read the machine axis (x,y,z) and R parameter in Simple OPC UA Client. I used this example : https://support.industry.siemens.com/cs/ww/en/view/42014088 I already add some certificate to that example (coz at the first time I tried it, it doesn't have the certificate so it doesn't work). I already write the correct URL and namespace URI so it can be connected. The problem is, I can't read the data because I don't know what to write in "Variable Identifier" and the error message (StatusCode) is : BadNotReadable. I found the solution for that StatusCode, that I have to make the username and password as its authentication. So I added some programs to make this authentication, but it doesn't work too. Anyone have suggestion for me? Btw, I've tried to read the data through OPC Scout V10 and it works. Thank you so much for your help. |
Last edited by: Jen_Moderator at: 7/9/2018 1:58:32 PMOptimized link. Last edited by: AutoGen_2076697 at: 7/10/2018 4:13:25 AM |
|
Follow us on