9/4/2018 10:19 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi s2tamil, The CFC chart will not get updated with the new names from the DB. When you compile the program, you will receive errors. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
9/5/2018 7:51 AM | |
Posts: 14 Rating: (1) |
Hi Oreca, So i have to change the text manually in each Charts ,is it Correct? |
9/5/2018 8:52 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi, No, you have to delete the interconnection and reconnect...Easiest is to compile the CFC program so you will see where the errors are located, then you have to adapt them one by one.. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on