9/17/2018 7:32 PM | |
Posts: 10 Rating: (0) |
Dear Sir , I am having issue with the GSD file data addressing.Our company was using acid dosing pump with profibus motor. Old motor was spoil and we bought the new acid dosing pump.The problem was old motor GSD file address and new motor GSD address was not match.We are not able to do the new profibus address in our S7-400 plc because of the data address will crash.If that have any possible chance to do some other to control the this acid dosing pump.Currently we are doing the manuall y top up the acid.With the profibus we can set the acid flow liter/minute from HMI.Now what we do is calculate the liter/ hours to liter per minute. Thak for the advice. Thank And Best Regards, Zayya. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/18/2018 10:28:10 AMNew subject after splitting |
|
9/18/2018 10:29 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
Closed cause question posted twice. The second thread with the subject Old GSD file and New GSD file not same address. is published within the conference Communication / Networks. Best regards, Jen_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on