9/6/2018 5:26 PM | |
Posts: 24 Rating: (0) |
Siemens s7-200 old SIEMENS USB/PPI MULTIMASTER CABLE 1P 6ES7 901-3DB30-0XA0 S C-C3VE4176 E-STAND:06 I want driver for this cable For Windows XP for communucation ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/7/2018 7:11:41 AMNew subject after splitting |
|
9/6/2018 6:18 PM | |
Posts: 24 Rating: (0) |
It's not working ..I just installed Windows XP and connected not working i want driver for cable |
9/6/2018 6:26 PM | |
Joined: 12/18/2014 Last visit: 6/29/2024 Posts: 33260 Rating: (4115) |
Read this. MicroWin 4.0 SP9 is for WinXP SP3 (32-bit). Attachmentreadmeb.doc (349 Downloads) |
9/6/2018 6:26 PM | |
Posts: 24 Rating: (0) |
If I click communications in step microfinance it showing Error:port could not be opened or is being used by another application |
9/6/2018 8:30 PM | |
Joined: 9/27/2006 Last visit: 6/29/2024 Posts: 12264 Rating: (2673) |
Hello Usainbolt; This used to happen when serial ports were in more frequent use for PLC programming: outside programs could, and would, capture the serial port of your PC for their own use, and refuse to release it when your program needed it. This was a frequent problem when you were programming a Rockwell PLC on the same PC when you were opening Step 7, RSLinx would capture the serial port and Step 7 could no longer access it, until RSLinx was closed. See if the suggestions in this discussion can help you today: https://support.industry.siemens.com/tf/ww/en/posts/micro-win-problem/126319/?page=0&pageSize=10 Hope this helps, |
Follow us on