11/9/2018 6:08 AM | |
Posts: 3 Rating: (0) |
Hello comrades, I have another question about installation of CMC package to the machine. Is it possible to install the project automatically with options that were configured earlier to some external file for example production planning specialists? Let me explain. For example we have the machine "xxx" that must have options 1, 3, 6, 7 (selectable form list of options during manual installation of the project). Another machine "yyy" must have another options respectively. Operator inserts, for example, USB with project and some external file of configuration into NCU and installation starts and finished automatically according to the preselected options. By which means of CMC Expert it can be reached? Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/9/2018 2:03:20 PMNew subject after splitting |
|
Follow us on