(0)| 11/19/2018 12:56 PM | |
|
Posts: 1 Rating:
|
Hi, having difficulty with analog input A1 using a 0-10 bar pressure transmitter. Powered by 24v dc and output signal 0-10 vdc. Pressure is reading max 5 bar with gauge but my return signal is 10v dc or higher. 0v dc are tied together - power supply and pressure transmitter. when the voltage does get in range system switched rapidly in and off evening with analog trigger vault of on at 350 and off at 570. As soon as signal drops below 570 system starts. First I just need to get a decent signal. The analog input stays either at 1000 - 10v dc or 765 - 7.65 vdc even with system pressure almost 0 bar off gauge. This is the second pressure transmitter and am getting same result with both. Any help would be appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/19/2018 2:57:35 PMNew subject after splitting |
|
Follow us on