1/18/2019 6:31 PM | |
Posts: 8 Rating: (0) |
thank you i didn't know i should put in term mode to use freeport, now i have another issue i can upload to the plc with no problems but it seems it's connected to a literally USB port i mean when i open configuration and connections i just saw USB the problem is that nor realterm nor other programs detect that port ¿is there a way to change that weird USB to a COM port? I just installed the ch340 driver and i've looking for some solution ------------------------------------------------------------------------------------------ |
Last edited by: rodch98 at: 1/18/2019 7:02:48 PMLast edited by: Jen_Moderator at: 1/21/2019 11:04:31 AMNew subject after splitting |
|
Follow us on