1/16/2020 11:53 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Hello, While configuring handwheel user need to set PLC inputs & axes DB bits in logic so as to set axis increment value, axis velocity, axis direction etc. etc. Please refer SINUMERIK 840D sl/840Di sl/840D/840Di/810D, Extended Functions manual topic Manual & Handwheel travel (H1) chapter 2.4 Handwheel travel in JOG, for more detail information. HTH |
This contribution was helpful to1 thankful Users |
1/16/2020 3:45 PM | |
Joined: 3/12/2015 Last visit: 5/16/2024 Posts: 533 Rating: (15) |
Thank you PISCEAN but the problem was a bit simpler than that, i checked the signals and i noticed that the voltage didnt match up so i opened the handwheel and found that the internal connectors are broken. im going to solder the broken conectors tomorrow |
This contribution was helpful to1 thankful Users |
Follow us on