(1)| 12/20/2017 6:52 PM | |
|
Posts: 42 Rating:
|
Any reply here guys please for the IOT function to be used as WAN network ??? |
| 12/26/2017 4:14 PM | |
|
Posts: 439 Rating:
|
Hello Adham, If you plan to use the IOT for other purpose than to connect S7-1200, for example communicate with cloud, right. If you only want to connect your S7-1200 between each other, why don't you use product design for this application? Siemens have many product for IP-based remote communication, please see below link. You can use the CP1243-7 of the S7-1200 or Scalance M and S. 6GK7243-7SX30-0XE0 COMMUNICATION PROCESSOR CP 1243-7 LTE US 6GK7243-7KX30-0XE0 COMMUNICATION PROCESSOR CP 1243-7 LTE EU I prefer Scalance M and S since they provide access to the whole local network compare to the CP1243-7 giving you access to CPU only. Wired connection: 6GK5612-0BA10-2AA3 SCALANCE S612 Wireless connection: 6GK5876-4AA00-2BA2 SCALANCE M876-4 (EU) 6GK5876-4AA00-2DA2 SCALANCE M876-4 (NAM) There are many application example on SIOS. Setting up a secure VPN Connection between SCALANCE M-800 and SSC Using a static IP Address Yes, maybe it will be a bit more expensive, but those products are design for this purpose, reliability will come with it. This is an industrial application anyway, right? Best regards, Hugo |
This contribution was helpful to
|
|
| 1/26/2018 12:41 PM | |
|
Posts: 1410 Rating:
|
The CP1243-7 is not an open solution, as far I know. It can work just with Telecontrol Server Basic on the other side. |
Follow us on