10/29/2020 11:59 AM | |
Joined: 2/12/2018 Last visit: 9/26/2023 Posts: 22 Rating: (0) |
@ Denilson, Thank you so much for your popUp example! +++++ now can somebody kindly point out how to solve the following issue: I managed to create a popup faceplate with a toggle button in a screen (toggle the visibility of the faceplate). the code was splitted (creating the PopUp in Global definiton ) , (see attachment). then a button to toggle the Visibility porperty (in Script function) Now the close button in the title bar of PopUp will cause the PopUp to be closed permenantly and it cannot be reopened with the visibility property, and I need to keep the popup faceplate flexibly movable, how to merge this two points (CanMove: enabled & CanClose buttong : hidden) on page 580 Reference: WinCC Engineering V16 - Runtime https://cache.industry.siemens.com/dl/files/780/109773780/att_1007135/v1/WinCCVisualizingProcessesRTU_en-US.pdf The following property WindowFlags can be set, but I didn't manged to set both (CanMove: enabled & CanClose buttong : hidden) in the document there was no explanation about the syntax in order to set two or more values (if that possible!). Trying to look for something in the help of TIA 16, I came up with the same information as in the documents above. Thanks in Advance for your Tips ------------------------------------------------------------------------------------------ |
Last edited by: Optimistic at: 10/29/2020 12:27:42Last edited by: Optimistic at: 10/29/2020 13:59:05Last edited by: Jen_Moderator at: 10/29/2020 14:06:28New subject after splitting |
|
Follow us on