12/3/2020 12:48 PM | |
Joined: 9/23/2005 Last visit: 10/29/2024 Posts: 4351 Rating: (1451)
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Alarm messages are an important tool for operation diagnose of process and system events. There is many variations about alarm and alarm view object settings. Here there is two variants of then: pending and logged alarms. Configuration main steps:
TIP:to insert dynamic text to the alarm text (e.g. variable values as part of the text): select the alarm text for edition, right click mouse, "Insert parameter filed...", and add a tag Project (.zap16 ziped as .zip) AttachmentAnalogAlarm.zip (713 Downloads) |
Last edited by: Denilson Pegaia at: 12/03/2020 12:56:21Last edited by: Denilson Pegaia at: 12/04/2020 11:24:01Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on