1/27/2021 10:26 PM | |
Joined: 3/7/2014 Last visit: 3/21/2024 Posts: 27 Rating: (0) |
Hi Does anyone know how to make a "cnc program" and save it in a s7-1200 plc. The 2 axes should make a simple movement (like a V, with an arc at the bottom of the tip.) I have the program from a cnc controlled machine (see attachment), but how is it stored in the PLC? I think i can use the the web interface to transfer a recipe ti it, but i dont. know how to store it, and what format it should bee. I have control of the hardware and the PTO setup, but need some information about the "program" itself that should control the movement. Attachmentcnc program med 3 program valg .txt (235 Downloads) |
Follow us on