10/15/2016 5:51 AM | |
Joined: 3/2/2015 Last visit: 5/8/2024 Posts: 5 Rating:
|
Can you please suggestion the overall of IOT2020....and IOT 2040 1) Over all architecture 2) Target applications and their configuration 3) Knowledge required ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/18/2016 12:06:59 PMNew subject after splitting |
|
10/17/2016 4:43 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating:
|
Hi MASS_1200, 1) some general information and an overview you can find in the two documents here. 2) For instance a gateway between the field devices and cloud platforms is a possible application. Configuration of the application is to you. We provide an example image with some integrated functionality, but the applications have to be developed by the costumer. 3) It depends on the application you want to develop. But in general some Linux knowledge is required. C/C++ knowhow is also not bad to have for programming the device in Eclipse. |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/5/2017 11:30 PM | |
Posts: 2 Rating:
|
Hey guys, Are both IOT2020 and IOT2040 UL listed? where can I find info about it in the website? Thank you |
6/6/2017 8:19 AM | |
Posts: 215 Rating:
|
You could check Siemens support pages for further details, like the operating instructions. Chapter 7, Technical specifications. |
1/8/2019 10:37 AM | |
Posts: 33 Rating:
|
Can IOT 2040 works on Windows 10? |
Follow us on