8/17/2021 8:36 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875)
|
Hello, Please refer attached sheet. In PCU 50.3, 2 nos. batteries will be there, one for PCU BIOS & second one for MCI board. MCI board battery is NCK battery i.e. it backs up NC, PLC data stored in SRAM. So you need to replace battery which is connected to MCI board. HTH P. S. - In order to share with you battery article number, please attach ths snap shot of PCU50.3 here. {Article number which you specified doesnot exist, so its better if you attach the snap shot of PCU50.3 nameplate sticker.} AttachmentNCK MCI board battery.pdf (503 Downloads) |
Last edited by: PISCEAN 2010 at: 08/17/2021 09:06:12P. S. added |
|
This contribution was helpful to1 thankful Users |
8/17/2021 1:03 PM | |
Joined: 3/11/2020 Last visit: 7/9/2024 Posts: 13 Rating: (0) |
Hello Please open the attachment. As per the instructions i opened the cover and it seems like the same battery on top is connected to the MCI PCB. Not directly, but connector from the MCI board and connector from battery is close to each other on anotber PCB just below the battery.. No other battery is visible nearby and no battery on MCI PCB. Regards, AttachmentScan 17 Aug 21 · 01·41·05.pdf (446 Downloads) |
8/17/2021 2:00 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875)
|
Hello, I suggest you to contact OEM or your nearest local Siemens support center, since exact PCU 50.3-C article number is not available on sticker. Moreover from construnction point of view, it also looks different. I found out below details of battery which please get confirm before ordering. (image attached here with for your ready reference) Article number A5E00331143 SIMATIC PC, spare part Lithium-Metal CMOS Battery 3V, VARTA CR 1/2 AA; Battery type: LM188; for Box PC 620/627/827/B/C/D; Box PC 820/840/V2; Panel PC 670/677/B/C/D; Microbox PC 420/427B; IPC427C; PG720/740/760, Duty to supply information according to article 33, REACH regulation: the product contains the following substance from the candidate list in concentrations exceeding 0.1% by weight: 1,2-Dimethoxyethane, Ethylene glycol dimethyl ether (EGDME) (CAS 110-71-4; EC NO 203-794-9) |
This contribution was helpful to1 thankful Users |
8/24/2021 9:38 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875)
|
Hello, Please refer attached files, explaining how to take & reload series data back up. Please note, you need to re-connect new battery within 10 minutes (time depends on energy stored in super capacitor inside PCU which proiveds power to SRAM) from the time you disconnect NCU battery. HTH P. S. - Ofcourse you need to replace battery when power to Machine & PCU is OFF/shutdown. AttachmentHow to reload series start up files using OP.zip (498 Downloads) |
Last edited by: PISCEAN 2010 at: 08/24/2021 09:40:09P. S. added |
|
Follow us on