2/13/2024 6:29 AM | |
Joined: 1/21/2013 Last visit: 6/14/2024 Posts: 2886 Rating:
|
Hi Franck1234, In several programming languages, including JavaScript, the backslash is used as an escape character to allow the use of special characters in strings. So to create a backslash, you have to type two. But of course, since you are not typing into a string within a script, but into a system-defined input field, you should not have to worry about this. You should check if this problem still occurs when using the latest image version. (Even if you are using V18 for engineering, you can use the V19 image on your device). If the problem still occurs with the latest version, you should contact Siemens Technical Support by creating a support request. Kind regards |