7/3/2009 9:23 AM | |
Joined: 4/24/2006 Last visit: 5/31/2024 Posts: 8664 Rating: (1154) |
Dear Wincc, Are you using the right parameters? P700 = 5 P2011 = unique address Best regards, Wizard |
7/3/2009 9:39 AM | |
Joined: 6/3/2009 Last visit: 2/8/2024 Posts: 101 Rating: (7) |
Dear Wizard Yes, i had set P700 --> 5. But one thing i am using Profibus module with the drive. |
7/3/2009 9:52 AM | |
Joined: 4/24/2006 Last visit: 5/31/2024 Posts: 8664 Rating: (1154) |
Hi Wincc, I'm going to give you some bad news Do not shoot me, I'm just a messenger. It will not work. See this thread I found: /tf/WW/en/Posts/20481 Perhaps you should use RS232 to connect AOP: http://support.automation.siemens.com/WW/view/en/17524694 Best regards, Wizard |
Last edited by: Wizard at: 7/3/2009 11:17 AM |
|
7/3/2009 12:16 PM | |
Joined: 6/3/2009 Last visit: 2/8/2024 Posts: 101 Rating: (7) |
Dear Wizard Thank you for replay. I won't shoot you and you had givven me a solution. Thankyou onc again. |
7/3/2009 1:11 PM | |
Joined: 4/24/2006 Last visit: 5/31/2024 Posts: 8664 Rating: (1154) |
You are welcome. Did you try without profibus module? To be sure that's the problem. Best regards, Wizard |
7/6/2009 7:16 AM | |
Joined: 5/28/2008 Last visit: 5/29/2024 Posts: 4507 Rating: (837) |
Hello, Then the problem is in the socket of the AOP mounted on the profibus module! |
Ayman Elotaify |
|