7/15/2021 3:01 PM | |
Joined: 10/11/2006 Last visit: 6/18/2024 Posts: 5861 Rating:
|
Hello, with V17 there is the possibility to change at end of cam. Direct synchronization at the end of the cam With the "MC_CamIn.SyncProfileReference" parameter = 5 you change another cam or the current cam with a new scaling at the end of the active cam. The "synchronous" status remains set. For more detailed information on direct synchronization at the end of the cam, refer to section "Direct synchronous setting with "MC_CamIn" at the end of the cam (Page 77)". 5.7.5 Direct synchronous setting with "MC_CamIn" at the end of the cam (S7- 1500T) https://support.industry.siemens.com/cs/de/en/view/109781851 With V16 you have to start the MC_CamIn at the right masterposition and you have to calculate the rigth "sysnchronous position" and using maybe an offset for MC_CamIn. 5.7 Synchronization (S7-1500T) |
With best regards, |
|