9/12/2022 6:17 AM | |
Joined: 3/30/2020 Last visit: 7/31/2024 Posts: 4665 Rating:
|
Are you using an S7-1200 with firmware V4.5 under Step7 V17? If YES then see the following link: As alternative select a firmware V4.4 PLC in your project. If the answer was NO to the above question.. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
9/19/2022 1:25 PM | |
Joined: 8/3/2009 Last visit: 7/31/2024 Posts: 13425 Rating:
|
Hello Ebubekir97 In the technical data of the Panel is also listed that a communication to S71200 is possible. https://support.industry.siemens.com/cs/ww/en/pv/6AV2124-0XC02-0AX1/td?dl=en Bye Murof |
If this Information really helps, you could use the Rate function |
|
9/21/2022 7:17 PM | |
Joined: 3/30/2020 Last visit: 7/31/2024 Posts: 4665 Rating:
|
Hello. Are you attempting to do a simulation? Review the following FAQ which discuss all combinations of simulation: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
9/22/2022 6:29 AM | |
Joined: 8/27/2020 Last visit: 12/11/2022 Posts: 16 Rating:
|
My plc and hmı panel connected with profinet but ı dont understand this problem.What are you tell me ? |
Follow us on