4/5/2013 7:57 AM | |
Posts: 19 Rating: (1) |
Dear Sir, yes The drivers installed during installation ,the interface should used is RS232/PPI multimaster cable. best regards,
|
4/9/2013 8:03 AM | |
Posts: 19 Rating: (1) |
Dear Sir, i am still wiating your reply ! please a very urgent issue, cannot communicate with my PLC best regards,
|
4/9/2013 8:58 AM | |
Posts: 19 Rating: (1) |
Dear Sir, yes step 7 is installed before microwin installation. how can export my settings? the problem is cannot select PPI and all CP5711,CP5611,5512 and PC adapter etc.. is not shown in hardwre set PG/PC interface.when selecting add/remove button it show me that all is installed.afetr closing these options is not shown in the list. PLease see my project attached regards,
AttachmentToupri_1.zip (709 Downloads) |
4/12/2013 8:35 AM | |
Posts: 19 Rating: (1) |
Dear Sir, Still not foud PC/PPI cable in our Set PG/PC interface!!!!! please can someone help me |
4/12/2013 9:06 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello Johnny77, Have you seen this thread: /tf/WW/en/Posts/81753#top Or this thread: /tf/WW/en/Posts/75509 Perhaps it might help. Best regards, Wizard |
4/12/2013 10:07 AM | |
Posts: 19 Rating: (1) |
Dir Sir, i tried all possibilities before without sucess please any other suggestion?? or any extra driver software for ?? thanks in advance |
4/12/2013 11:46 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello Johnny77, Ok, I guess you already tried to uninstall Step 7 MicroWin and installed it again. Another possibility would be to install Windows again. (Please use a complete Windows, not the preinstalled on HP) Or before installing Windows again, you could start a Support Request (and let us know the result) Best regards, Wizard |
10/10/2018 11:07 AM | |
Joined: 12/2/2015 Last visit: 5/28/2024 Posts: 64 Rating: (7) |
In my case, I firstly installed MicroWIN, and then Step 7 and then I chose Serial cable RS232 and chosen correct com number. Try this: https://support.industry.siemens.com/tf/ww/en/posts/microwin-4-0-9-25-installation-problem/81753/ |
Last edited by: LuWiack at: 10/10/2018 11:14:14 AM |
|
Follow us on