6/20/2014 12:31 PM | |
Posts: 15 Rating: (0) |
Project File Attached |
Last edited by: patultimate at: 6/20/2014 2:25 PMDeleted project file... |
|
6/20/2014 12:45 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713)
|
Hello, The program compiles without error at my pc. I noticed it's about a 224XP CN Maybe it helps if you download and install the latest version of STEP7 MicroWIN V4.0 SP8 and SP9 My settings are attached. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
6/20/2014 2:14 PM | |
Posts: 5225 Rating: (1187) |
Marc, I can confirm the same. Windows 7, Microwin V4.09. @patultimate: There is one trick left to do. Attached is a ZIP file. This is password protected.. I'll send you the password by "Private Message". Inside the ZIP file is the export of the project you gave us to work with. The file is called "project export.awl". 1. Open Microwin - the version software does not matter. 2. Go under FILE > IMPORT. 3. Select the AWL file and import this into a new project. 4. Ensure the right PLC type is selected. 5. Save the project. 6. Compile that file as is. Let us know if this worked.. please. Greetings. w Attachmentproject export.zip (249 Downloads) |
6/20/2014 2:31 PM | |
Posts: 15 Rating: (0) |
Received same error while importing, see attachment I will update Microwin and see what happens, thanks
|