7/16/2011 4:00 AM | |
Posts: 1 Rating:
|
i want configuration s5 cpu 928b with im 308c as profibus master conected to 10 ET200.i wanna know what hardware & software i need to do that? |
7/16/2011 2:42 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, The manual is here: http://support.automation.siemens.com/WW/view/en/1498610 |
Best regards |
|
2/4/2013 9:31 AM | |
Joined: 8/25/2006 Last visit: 9/16/2025 Posts: 2218 Rating:
|
Hello. Try to reinstall ComProfibus, but when start setup don't use autorun from CD. Start 'setup.exe' fromCD:\compbv51\Disk1, not from the root of CD. Then installHF2(first unpack .exe to the HDD). Then installHF3, also first unpack .exe to the HDD and run 'setup.exe' from directory ..\COMPROFI_V5123\COM_PB\Disk1.
|
3/1/2013 9:26 AM | |
Joined: 9/9/2012 Last visit: 9/6/2025 Posts: 11 Rating:
|
hello every body i configure master im308c and slave im 153-1 in both com profibus software 3.3 and 5.1.2.2 but no communication between master and slave so plz any body tell me right parameter for im153-1. and find the configured .et2 file with com profibus 3.3 AttachmentNew Folder.zip (682 Downloads) |
Last edited by: Deepak Pradhan at: 3/1/2013 9:26 AM |
|
10/5/2017 11:38 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by alnashar is split to a separate thread with the subject Need com profibus 5.1. Best regards |
Follow us on