3/5/2016 9:58 AM | |
Posts: 5225 Rating: (1191)
|
Yes. |
3/5/2016 12:21 PM | |
Posts: 5225 Rating: (1191)
|
Much of the stuff is done by memory by now. What will also help you two guys.. If you do like my style of teaching... Request the system to show posts I was involved in by my user name. You can then narrow the search by "motion control" or "HSC" or something like that. w |
This contribution was helpful to1 thankful Users |
3/5/2016 7:55 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
If you're not using the Z output don't worry about gated or ungated. That just describes the relationship between Z and A&B pulses. If it's an open collector then it's NPN and you will need to do as William mentioned in his post, add a pull-up resistor. |
Follow us on