10/12/2018 11:19 AM | |
Posts: 3 Rating: (0) |
Hello, I am using Starter V5.1 in combination with S120 drive. Now I will use DCC in Starter program. Therefor I bought a license for it. I got a USB key with the license. After installing I started the License Manager. Then I copied the License key to my Windows C: directory. But by using the Starter program DCC is not activated. It’s visible, but nothing appears when I click on a DCC project, even so when I will insert a new DCC chart. What did I wrong? Regards Leen ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/12/2018 11:43:24 AMNew subject after splitting |
|
10/23/2018 11:45 PM | |
Posts: 1 Rating: (0) |
There must be an error that is why the problem is happening. If I believe, this must be an issue of the error 0142 and the Dell error code 2000-0142 could be a possible reason behind this. Please make it sure. |