12/2/2013 1:08 AM | |
Joined: 1/24/2008 Last visit: 9/29/2024 Posts: 30 Rating: (1) |
Hi, I have a system with a cpu 1214c (fw 2.2) , cp1242-7 (fw V1.3.3) and TIA v12 sp1. I use a SIM card that I have already tested it sending sms in a mobile phone in the same local without problems. I want to use the system to send and receive sms. The system doesn't answer to the cpdiag sms command sent by a mobile phone. I try to send a sms from the system using my program.ap11 (tested successfully some months ago ), but without results. The led DIAG of cp is always blinking in green. The others leds of the cp are off. The led RUN of cpu is green. With TIA online, I run the “online & diagnostics” in the Local modules CP 1242-7 and the result is in attachment. Meanwhile, I did some attempts to solve the problem, but without success: I upgrade the program from .ap11 to .ap12 I also tried the TIA v11 sp2 update 5 (HSP CP1242-7 V1.0 installed). I will appreciate some suggestions to solve the problem. Thanks in advance, MLima Attachmentdiag of cp1242.pdf (344 Downloads) |
12/2/2013 2:58 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Hi, you could look at the operating instructions for the CP here. At page 22 there is an explanation for the LED status. Maybe this helps! Regards.... |
12/2/2013 6:17 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
you already tried to fully reset your S7-1200? which test-sms have you send? you only got the green led flashing and the others LED are not on? and you can send an sms with your mobile? --> the manual says there is no configuration. perhaps try to use another head-plc if you have one at hand? (as i said: try to reset) it can also be possible that you have made the wrong configuration/program to login? Please refer also to the application example here |
Best Regards, |
|
12/5/2013 1:08 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
What about the other LEDs at the CP? |
12/9/2013 4:12 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Then I guess we have to check your hw-config and your parametrization of those TC blocks. |
Follow us on