6/4/2021 9:34 PM | |
Joined: 3/31/2016 Last visit: 6/5/2021 Posts: 3 Rating: (0) |
Hi, ERROR INSTALLATION TIA PORTAL V1720:10:02 | OK ClassicCompAfterUninstall () Complete 20:10:03 |ERROR AdsWorkerForeignExe::GetInstallResult(): - 1603: assuming unknown error, because return value is not in OK-list which is only defined. Please check the corresponding log file for more detailed information 20:10:03 | FAIL! SetupUnit (URLRewrite2) Failed Foreign AddLocal Is there anybody who can help me ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/07/2021 08:42:57New subject after splitting |
|
This contribution was helpful to1 thankful Users |
6/7/2021 9:07 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
can attach the logfile of the failed component? |
10/15/2021 1:04 AM | |
Joined: 4/29/2015 Last visit: 5/17/2024 Posts: 5 Rating: (0) |
I have got the same error ERROR AdsWorkerForeignExe::GetInstallResult(): - 1603: assuming unknown error, because return value is not in OK-list which is only defined. Please check the corresponding log file for more detailed information During Tia v17 Unified installation under Server 2018 OS I attach the lig file. Please, could anybody help me? AttachmentSIA_STEP7_S7FPLUS_WINCC_ADV_V17@21-10-14_15-10-31_AFTERREBOOT_summary.txt (790 Downloads) |
8/14/2022 10:41 AM | |
Joined: 7/23/2022 Last visit: 6/5/2023 Posts: 1 Rating: (0) |
I have the same problem I'm using parallels windows 11 MacBook Air M1 AttachmentSIA_STEP7_S7FPLUS_WINCC_ADV_V17@22-08-14_09-42-03_summary.txt (527 Downloads) |
8/15/2022 7:36 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
please the complete logfile! Win11 ARM not supported for TIA Portal |
Follow us on