4/8/2010 6:37 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Thanks Graeme... This was something which I didnot found in Manual or any other forums.... Your help is appriciated.. Thanks & Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
4/29/2010 8:45 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Hi Graeme, You gave good explanation regarding F022 Now Please give some details for F001 also. This fault is also being headache from some time. Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
11/20/2012 2:06 AM | |
Joined: 11/26/2008 Last visit: 11/6/2014 Posts: 8 Rating: (0) |
Hi Vithani, Just curious did you find any solution the F001 problem? I am facing a similar one and it just comes up sporadically after a couple of weeks. |
"The most important thing is not to stop questioning." Albert Einstein |
|
2/21/2014 8:59 AM | |
Posts: 4 Rating: (0) |
Hi there, i found this tread since we are facing a similar problem coming up only some times. Special the A 0522 error followed by the F022 I have some additional questions. - Power supply is actually provided by a Sitop power supply. So if the Inverter is switched off the PB Modul is still under power and will not cause any faults. - Shall we change the power supply and take the 24 VDC from the inverter instead ? Is this your sugestion ? - Can you explain what makes the difference ? Many thanks in advance |
10/1/2015 4:14 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Allow me to share my recent experience with F022 and MM440. Suddenly the MM440 got that error. No way of reset it with or without motor's and breaking resistor's cables. Tried with replacing a new power block. The reason was missing 24VDC from inverter main card board 6SL3352-6BE00-0AA0. That voltage is going to 'supply' the IGBT's board (Sorry I don't have right now the MLFB number of it). Right now the MM440 is working with the same 6SL3352-6BE00-0AA0 board, just we give external 24VDC (external power source) to the IGBT's board. BTW we tried to use the 24VDC from the drive with no result. Best regards, Hristo Mihalev |
This contribution was helpful to2 thankful Users |
6/3/2016 4:57 PM | |
Posts: 1 Rating: (0) |
I am having this same issue but cannot find any documentation on what the 6 terminals but the fan relay you are referring to do. They are labeled 1-6 and I cannot find any internal drive circuit diagram that would state what is 24vdc and what is common. |
6/4/2016 6:08 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please check your drive MLFB number & size. |
6/18/2020 10:46 PM | |
Posts: 1 Rating: (0) |
Measure the input voltage and compare it with the data plate of the inverter. may it is low, so the supporting dc link volt will indicate alarm. |
Follow us on