11/28/2011 4:54 PM | |
Posts: 44 Rating:
|
Hi I have been having some of the same issue's I think if you follow this thread, although the application is different, the questions are the same /tf/WW/en/Posts/65197#top With Gorps last answer to me, I believe I am sorted - for today |
11/30/2011 2:03 PM | |
Posts: 5225 Rating:
|
To Gorp, Thank you for the HSC example. I have downloaded it and had to convert from TIA V10.5 to V11.0 SP2. I could not run the code as I do not have hardware at the moment. There is a question though about the HSC input on the CTRL_HSC block as used in FC1. According to documentation..
Gorp, in your example the HSC input has a value of 0. If I understand correctly this value should be 1. See in the PDF file where I get this number. But also.. I have opened a new project and see that this hardware identity can be different between projects. See the PDF why I say this. Therefore it is the safer route to use the system constant that has the actual value of the hardware identity. Please can someone verify my opinion for me? To Thome_sc: I am sorry for us letting you down like this. There are so many things that needs to be considered that may go wrong when using HSC. I suggest you use a button (24V) connected to the input corresponding to the HSC you wish to use. I am aiming to isolate where your problem is.. inside the PLC or outside the PLC. Please give us as much info as you can.. like a piece of your program and connection drawings. I am sure we are overlooking something. Greetings, AttachmentQ_what should HSC be for HSC_CTRL.pdf (896 Downloads) |
This contribution was helpful to
1 thankful Users |
12/7/2011 3:29 PM | |
Posts: 50 Rating:
|
Hi .Iam working on a similar project calculating the velocity of a conveyor in M/min.It's the first time iam using HSC in S71200 .It is very simple programm but its running.That means that i have load the project to a CPU 1214C DC/DC/DC also i have connect and an ecoder 360PPR.I have set the HSC as frequency type of counding.
AttachmentFEEDER.zip (772 Downloads) |
This contribution was helpful to
3 thankful Users |
12/8/2011 12:35 PM | |
Posts: 15 Rating:
|
Hi, attached is configuration example. hope this mayhelp you to solve ur queries... understanding the basics is too important.... BR sankar AttachmentConfigurationExample.pdf (906 Downloads) |
Follow us on