10/28/2013 10:25 AM | |
Posts: 29 Rating:
|
Thanks to both... I: - Allowed activation of OS on ES - Give IP addresses: - PLC: 192.168.1.25 - ES: 192.168.1.30 (IP address of the PC where I'm working) - OS: 192.168.1.20 - MAC protocol is unchecked - Recompiled OS using TCP/IP connection. AS address configured 192.168.1.25 - In WinCC / S7 protocol suite I choosed PLCSIM.TCPIP.1 (it was already chosen) - Downloaded HW, NetPro & SW to PLCSim - Started OS simulation And it did work. When I logon it appear a message saying: "Authentication was performed on this computer due to access problems" (Why?). But I access the program and I can test it, so many many thanks!! The problem was the Named connections (I think), son nice :) Now I'm going to test with the real CPU, that has arrived today. I've seen next document: https://www.swe.siemens.com/italy/web/AD/ProdottieSoluzioni/Sistemiautomazionenew/Eventi/Documents/presentazioni%20simatic%20live/PCS7MultiprojectEngineering.pdf Where, in page 10-11 (porject like mine), it is said that a disadvantage of a multiproject like this is: Testing AS and OS during the project engineering is performed on separate computers. I think this is related to the work of the OS as server itself, not related to the behaviour of the runtime. Is that correct? Thanks again! |
Last edited by: manute at: 10/28/2013 10:29 AMLast edited by: manute at: 10/28/2013 10:28 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on