5/13/2019 4:50 PM | |
Joined: 12/18/2014 Last visit: 9/3/2025 Posts: 35917 Rating:
|
Here is a program proposal. I divided the pressure range that the sensor outputs into 3 sections. Each section can then be assigned its own weighting factor in the associated mathematical instruction. In the proposal, it is in the first area 4 kg, in the second 8 kg, in the third 12 kg. The fourth mathematical statement then determines the total. You then have to determine the right area and factors yourself. The example should only show you the way. AttachmentTank.zip (1075 Downloads) |
This contribution was helpful to
1 thankful Users |
5/14/2019 6:21 AM | |
Joined: 12/18/2014 Last visit: 9/3/2025 Posts: 35917 Rating:
|
I'm looking forward to the feedback ... |