7/30/2016 1:15 PM | |
Posts: 5225 Rating: (1191)
|
Hi. Attached is a follow-up project. Added in this project the PWM is controlled as set by the analog input. The DC motor now has direction and speed control. User <engco> will also benefit from this sample, The design was done with TIA Portal V13 SP1 Update 9 but set to compatibility mode for TIA Portal V13 SP0. The code is untested. Highlights to note.. B - NOT SPECIFIC TO TOPIC Some instructions on loading the project into the PLC.. Project is made available under Creative Commons Licensing - with the request that the licensing be kept in place and it to be stated where the base code originated from (web site & author). The community is welcome to make additions and add to the authoring list. Forum members are encouraged to make contributions. Good luck. AttachmentExp1x2.zip (304 Downloads) |
Last edited by: William_B at: 7/30/2016 2:28:18 PMAdd instructions on loading PLC |
|
7/30/2016 8:14 PM | |
Posts: 5225 Rating: (1191)
|
Some more general (hand drawn) notes ..AttachmentPWM_usage.pdf (347 Downloads) |
This contribution was helpful to1 thankful Users |
8/1/2016 1:42 PM | |
Posts: 38 Rating: (0) |
Hi Wiliam, Thank you for your time and the valuable contribution. As per the attached pic the configured code for reading the speed is not working as I downloaded the project and test it. Please advice if the project need any addition. Regards.. Okod. AttachmentExp1x2 back.pdf (272 Downloads) |
8/1/2016 1:55 PM | |
Posts: 38 Rating: (0) |
Also see this.
Attachmentmotor speed.pdf (302 Downloads) |
Follow us on