10/20/2023 7:52 AM | |
Joined: 2/6/2022 Last visit: 8/9/2024 Posts: 9 Rating: (0) |
Greetings, i have problem with my DMU35M machine. When we bought machine there was a problem when you turn it on. I had "No NC ready" message on screen. Seller told me to keep it on for a few min then turn off and on. So I did followed his guide and did just that. Machine worked without any problem. In order to avoid long boot times, machine was rarely turned off. One day i came to work and i saw alarm, i cant remember what alarm was, but it was about Z axis. So i rebooted machine and i cant turn it on since then. Always "No NC ready". I have following alarms: 300200 NCK Drive bus hardware fault 700212 PLC_MSG BM CNC not ready for operation (drive, MMC or NCU) My setup is: SIMODRIVE 611, U/E-MOD. INT/EXT. 10/25KW 1P 6SN1145-1AA01-0AA1 SINUMERIK 810D LT-MODUL 2*15A+1*50A 1P 6FC5447-A00AA-0AA1 (SINUMERIK 810D CPU 810DE CCU1 SOFTWARE VER.2.4 1P 6FC5410-0AY01-0AA0) SIMODRIVE LT-MODUL INT. 2X8A 1P 65SN123-1AB00-0HA1 SIMODRIVE PW-MODUL INT/EXT. 1P 6SN1113-1AB01-0BA1 PCU 50, MMC101/102 Any help would be welcome to fix or diagnose this problem. I am a programmer and operator, but i have some knowledge and skill to do what is needed to be done in further steps of diagnostic.Thanks Dado Bojanic "This is a video of CCU led screen from the moment i turn on machine" AttachmentPictures.zip (244 Downloads) |
Last edited by: DadoBojanic1984 at: 10/20/2023 10:43:29Last edited by: DadoBojanic1984 at: 10/20/2023 11:00:56 |
|
10/20/2023 9:55 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating: (170) |
Hello DadoBojanic1984, please attach your files as an attachment and don't use ibb as a filesharing hoster. I can't open and check it, because the website is blocked. If you want to attach more than one file, you can create a .zip file. Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
10/20/2023 10:39 AM | |
Joined: 2/6/2022 Last visit: 8/9/2024 Posts: 9 Rating: (0) |
Ok let me edit quickly. |
This contribution was helpful to1 thankful Users |
10/21/2023 7:04 AM | |
Joined: 2/6/2022 Last visit: 8/9/2024 Posts: 9 Rating: (0) |
Is it the board inside 810d CCU? It connects from X130 to LT module 2x8A with 6SN1161-1CA00-0BA0 drive bus cable ?AttachmentCCU and 2x8a.zip (270 Downloads) |
10/24/2023 9:29 AM | |
Joined: 2/6/2022 Last visit: 8/9/2024 Posts: 9 Rating: (0) |
Finger pointed to X130 |
Last edited by: DadoBojanic1984 at: 10/24/2023 10:23:42 |
|
10/24/2023 9:30 AM | |
Joined: 2/6/2022 Last visit: 8/9/2024 Posts: 9 Rating: (0) |
right side drive-2x8 |
Follow us on