8/7/2014 9:41 PM | |
Joined: 1/21/2013 Last visit: 3/20/2024 Posts: 24 Rating:
|
KrunoT, The PCS7 V8.0 and V8.0 SP1 cannot be installed in the Windows 7 Professional. It can be installed in Enterprise (32 and 64 bit) SP1 and Ultimate (32 adn 64 bit) SP1. You can check the compatibility by means of the Compatibility Tool, please have a look: https://support.automation.siemens.com/kompatool/pages/main/index.jsf In the manual SIMATIC PCS 7 Read Me V8.0 SP2: The following operating systems are supported in PCS 7 V8.0 incl. SP2 : ● Windows XP Embedded Standard 2009 ● Windows XP Professional SP3 (32Bit) ● Windows Server 2003 SP2 Standard Edition (32Bit) ● Windows Server 2003 R2 SP2 Standard Edition (32Bit) ● Windows 7 Ultimate/Enterprise SP1 (32Bit) ● Windows 7 Ultimate/Enterprise SP1 (64Bit) ● Windows Server 2008 SP2 Standard Edition (32Bit) ● Windows Server 2008 R2 SP1 Standard Edition (64 Bit) http://support.automation.siemens.com/WW/view/en/89672900 |
8/8/2014 9:49 AM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating:
|
Hi KrunoT, you can order an Industrial Workstation from Siemens with Windows 7 Ultimate and PCS 7 V8.0 SP2 already installed. See the following link for more information: http://support.automation.siemens.com/WW/view/en/98164965 Regards jumo |
9/22/2014 5:33 AM | |
Joined: 8/29/2008 Last visit: 7/15/2024 Posts: 11 Rating:
|
I'm already test install PCS7 v8.0 on Win7 Pro 32bit. |
9/22/2014 7:40 AM | |
Posts: 14 Rating:
|
Hi Arashi, How did you pass first setup step when PCS7 software checking Windows version? KrunoT
|
9/22/2014 9:13 AM | |
Joined: 8/29/2008 Last visit: 7/15/2024 Posts: 11 Rating:
|
After install step running, i can't find any step about OS check. |
Last edited by: arashi at: 9/22/2014 12:56 PM |
|
Follow us on