3/23/2016 2:55 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Sorry, I have a few, but there are official and not allowed to share them...I got virtually b*tch slapped by the moderator for doing that once unintentionally However I found a link with some info: Pharma-food.de I think I may share this....
|
Last edited by: Oreca at: 3/23/2016 3:02:07 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/3/2016 8:07 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Official link: |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/9/2016 3:04 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
PCS7 8.2 Released for delivery! |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/9/2016 6:35 PM | |
Joined: 4/16/2012 Last visit: 10/16/2019 Posts: 2 Rating: (0) |
Old Step7 v5.5 SP4 Upadte9 for Windows7 , not for W10 |
4/9/2016 8:17 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
Correct, only "Clients" are released for Windows 10. I think we'll have to wait for at least SP1 in order to get the rest of the PC stations compatible with Windows 10. Sure there working on it. |
If I could help you, you can use the RATE button. Thank you. |
|
4/9/2016 8:49 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
One thing that disturbes me the most is the fact that PCS7 8.2 seems it does not support the "classic" library anymore (PCS7 7.1 SP3 blocks). So if you want 8.2, you have to re-engineer the plant with APL... Edit:What I mean: A customer who migrated from 6.1 to 8.1 recently without using new functions because its costed too much money is now stuck at 8.1.(looks like it). I told them the time would come that classic would not be supported, but didn't think it was so soon. |
Last edited by: Oreca at: 4/9/2016 8:50:35 PMLast edited by: Oreca at: 4/10/2016 9:28:46 AMIf I could help you, you can use the RATE button. Thank you. |
|
4/10/2016 9:24 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942) |
I've been working with APL for 3 years now..that was not what I meant, but what I meant was that a client has migrated five plant sections from 6.1 to 8.1, without using new functions, because engineering with APL was too much in regard to money. Now it looks like they are stuck at 8.1. Ive told them it was better to use APL and the time would come, but not so soon. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on