4/14/2020 12:27 PM | |
Joined: 5/24/2019 Last visit: 8/17/2022 Posts: 19 Rating: (2) |
Hello! I tried similar example to yours. I entered value 1, and the returned value is 256. |
4/14/2020 12:29 PM | |
Joined: 5/24/2019 Last visit: 8/17/2022 Posts: 19 Rating: (2) |
Here is the program. AttachmentAnalog_Example.zip (137 Downloads) |
4/14/2020 2:26 PM | |
Joined: 3/30/2020 Last visit: 5/9/2024 Posts: 4495 Rating: (942) |
@zbunic: Review the picture I shared last. The version numbers of the software shows the minor update versions too. PLCSIM is V15.1 update 1 (V15.1.0.1) for example. The screen capture you shared earlier only shows major version numbers. Please evaluate the versions of your software. There is a very high probability that you are not on the newest software updates. The below message comes up when your project is open. Known that the firmware is left at V4.2 as you have set it. The message indicate an internal update which would not happen if you and I have the same software updates. If you have doubt, re-install the PLCSIM with whatever last version is available to you. In the process of re-installation, there will be the option to repair the software if you already have it installed. Repair the installation. Plan B: In this way you can directly manipulate the analog input as if it is normal memory. |
Last edited by: qwazee at: 04/14/2020 14:28:01Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to4 thankful Users |
4/15/2020 9:37 AM | |
Joined: 5/24/2019 Last visit: 8/17/2022 Posts: 19 Rating: (2) |
Hello, I found the solution. I had to download an update for PLC SIM on this link: https://support.industry.siemens.com/cs/document/109764220/updates-for-plcsim-v15-1?dti=0&lc=en-WW This updated my PLCSIM from V15.1 to V15.1 Upd1 as it was in your image. Thank you everyone for your help. |
This contribution was helpful to4 thankful Users |
5/2/2020 1:24 PM | |
Joined: 4/6/2016 Last visit: 4/24/2024 Posts: 83 Rating: (15) |
Hello Everyone, Same problem I faced it resolved larer after PLSIM update. |
Many Thanks, |
|
Follow us on