1/15/2020 9:43 AM | |
Joined: 7/21/2016 Last visit: 5/25/2023 Posts: 2 Rating: (0) |
I need to replace a SIMATIC HMI KTP600 Basic mono PN with new for a client. I have asked for the project file which the client does not have. Is there a way to upload the project file from the HMI and download to the new one or do they need to revert to the company that supplied the equipment to get the source code? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/15/2020 20:09:16New subject after splitting |
|