5/14/2009 10:47 PM | |
Joined: 7/2/2008 Last visit: 5/16/2024 Posts: 928 Rating: (306) |
Hello, Interesting question form UMENCHO, Why would you change the CPU with the same one?! Do you have any INTF, EXTF or BF? If you don't have any faultand you just need to have spare parts then buy the CPU with same order number and keep it in stock. Why would you shutdown the plant?! I suppose Siemens CS knows more however I can't find a technical reason for not confirming that newer CPUs will run without error. Take a look at these links. http://support.automation.siemens.com/WW/view/en/19913888 http://support.automation.siemens.com/WW/view/en/24641526 http://support.automation.siemens.com/WW/view/en/25208203 http://support.automation.siemens.com/WW/view/en/22919199 Best regards. H-H |
2/1/2016 10:03 PM | |
Joined: 3/28/2015 Last visit: 5/15/2024 Posts: 721 Rating: (213) |
Hello, Successor product: If the only difference between the order numbers is the last digit of the middle block, then compatibility is ensured. CPU replaced by a successor CPU,it should work even if you not modify the H.W What should you watch out for when changing from one S7-400 CPU to another? |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
2/2/2016 8:39 PM | |
Posts: 4 Rating: (0) |
Thank you sir, I will study the manual and do it. Thank for your kindness. Thank And best Regards, Kyaw Zay Ya
|
This contribution was helpful to1 thankful Users |