12/12/2018 11:33 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33047 Rating: (4082)
|
Use mathematic instruction. If you enter the value via display, the value would be saved in a flash Memory. |
12/12/2018 11:49 AM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33047 Rating: (4082)
|
I must just go out of office. Later i will give you an example. |
12/12/2018 12:08 PM | |
Joined: 7/24/2017 Last visit: 2/1/2024 Posts: 8 Rating: (0) |
Thank you. I'm waiting your solution. |
12/12/2018 3:58 PM | |
Joined: 7/24/2017 Last visit: 2/1/2024 Posts: 8 Rating: (0) |
No. The set temperature will be between +10 and +30. |
12/12/2018 4:12 PM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33047 Rating: (4082)
|
In the attachment a possible solution. The setpoint from the HMI (or App) is polled to see if it is opposite the last stored setpoint. If so, then the current setpoint is stored. AttachmentStoring_Setpoint_from_HMI_Fail-safe_in_LOGO!_(automatically)_FS4.zip (669 Downloads) |