2/23/2009 1:34 PM | |
Joined: 7/8/2008 Last visit: 10/14/2023 Posts: 12 Rating: (2) |
Hello, We have multiple systems with same hardware, S7-412 FH and F IO Cards. I want to know if i have to order any runtime license for F-Systemalong with the hardware, as of now the material list that i have prepared does not have any runtime license. Below are the responses i read on this forum: /tf/WW/en/Posts/14056 Late: Hi, The RunTime is as far I know only a sticker for using the TUEV clarancy... So install only S7-Safety and CFC and you could do something with the Safety in the H-System. /tf/WW/en/Posts/4931 Late:Hi Swaminathan, As said by the Smurf you didn't need this anymore when you have S7 V5.3, so it is also not necessary to buy this package when you have S7 V5.3 or higher. For F-Systems you must buy the F-Package once and the number of copy-license for each system you use.
|
5/27/2009 11:44 AM | |
Posts: 1 Rating: (0) |
Hi Did you ever find out the answer to this query? I havea similarproblem. Cheers |