9/30/2019 6:08 AM | |
Joined: 5/25/2015 Last visit: 5/11/2023 Posts: 44 Rating: (1) |
Hello all, I want to setup Fault Tolerant communication between 2 Nos of S7 400H over Profinet . I have searched this forum and till now i only found this related link. I dont want to use Get Put communication here as it wont give me error on passive partner. Can you provide any application program , getting started manual for such cases. Also if i use AG_SEND & AG_RECEIVE, which CP Hardware address should i put for L_ADDR ( Hardware identifier) as this is going to be redundant comm . Active Partner : CPU 417-5H PN/DP 6ES7 417-5HT06-0AB0 CP 443-1 6GK7 443-1EX30-0XE0 Passive Partner : CPU 414-4H PN/DP 6ES7 414-4HM14-0AB0 CP 443-1 6GK7 443-1EX20-0XE0 |
Last edited by: Harish G at: 11/13/2019 12:39:20 |
|
9/30/2019 9:24 AM | |
Joined: 12/10/2018 Last visit: 5/26/2024 Posts: 109 Rating: (11) |
Hello Dear Harish please follow below link |
Last edited by: The Helping Hand at: 09/30/2019 13:42:53Optimized link. |
|
11/13/2019 12:41 PM | |
Joined: 5/25/2015 Last visit: 5/11/2023 Posts: 44 Rating: (1) |
Hello, Can anyone contribute to this? Which blocks should i use for Fault tolerant communication between S7 400 H. |