1/24/2018 4:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello sinumerkreza, From your circuit, 230 Volt supply is directly connected to drive, which should not be. You need to apply this power thru contactor which is controlled from K2 relay of A2 card. Power should be applied to drive only after enabling X:17 & X:18 comand i.e. drive start. & CR. Please refer the modified circuit in attachment. Set the field current first & check as per procedure explained in Start up. Best of luck. |
Follow us on