1/22/2012 10:55 AM | |
Posts: 2964 Rating: (478)
|
Hello... My suggesstion would be clear you NC and PLC properly first....Check this link.... /tf/WW/en/Posts/62589 Does your 810d is connected with PCU20 /pcu50 .....??? I never get the 9 in 7seg .but when I turn the S3+1 the 6 is appeared.==> this is used when your using software update from the PCMCIA card After you clear your NC(S3) PLC (S4)side i.e NC section side on the Leftt side..PLC section side i.e is on Right side after a proper clearing both side you should find 2 green LED's i.e on NC and PLC and 6 on seven segement display Check it ....after that you need to load your archive backups.... check this link /tf/WW/en/Posts/61649 Regards, Prakash |
1/22/2012 4:38 PM | |
Posts: 2964 Rating: (478)
|
Hello.... No archive are not stored in the PCMCIA card.... In your PCMCIA card the system software are only stored..... Regards, Prakash |
1/22/2012 5:39 PM | |
Posts: 7 Rating: (0) |
IT'S a PCU50 , I han't the archive files. in the HMI it not appariete. |
1/22/2012 6:50 PM | |
Joined: 3/19/2006 Last visit: 4/29/2024 Posts: 594 Rating: (78) |
write the NC and PLC archive to the NIC CARD ispossible al lot of 810D with PCU 20 has the Arc Strartup filesfrom the manufacturer on it AttachmentLOAD_PLC_From_Harddisk_PCU50.pdf (400 Downloads) |